LTE TDD

Carrier Information and Graphics

Indicates carrier or carrier aggregation information.

Channel Allocation

Waveform Information [ARB]

Carrier Aggregation/Component Carrier Selection Menu

Antenna Port Selection Menu

IQ Graphics

Spectrum Graphics

CCDF Graphics

Channel Allocation

Shows channel allocation resource map of the selected carrier.

The channel allocation map shows 1 frame (10 ms) configuration image at once. If waveform length is configured longer than 10 ms, GUI provides the map scrolling feature by selecting frames by menu.

Waveform Information [ARB]

The graphics capability is the same as the graphics under the Waveform tab, such as IQ, spectrum and CCDF graphics.

The waveform info graphics are not available for real-time waveform generation.

Carrier Aggregation/Component Carrier Selection Menu

Selects the target carrier layer.

SCPI Command

N/A

Dependencies

When a component carrier belong to carrier aggregation is selected in the upper pane, both Carrier Aggregation and Component Carrier selections are shown.

When a basic carrier (not belong to Carrier Aggregation) is selected in the upper pane, only Component Carrier is shown with read only. (or this menu selection is hidden?)

Range

Carrier Aggregation | Component Carrier

Initial S/W Revision

A.14.00

Antenna Port Selection Menu

The antenna menu selects the antenna port to show the target graphics.

When one antenna is configured, the antenna selection button is hidden.

IQ Graphics

IQ graphics of the selected carrier in the upper pane is shown in the lower pane.

IQ graphics has options to draw IQ image,

Power, I plus Q, and I and Q

Carrier Aggregation [Uplink/PRACH/Downlink]

This category selection is shown when a CA/CC carrier is selected in the upper pane category.

Shows IQ graphics of carrier aggregation layer of the selected carrier.

Carrier

Shows IQ graphics of the selected carrier.

Spectrum Graphics

Spectrum graphics of the selected carrier in the upper pane is shown in the lower pane.

Sample of Spectrum graphics:

Carrier Aggregation [Uplink/PRACH/Downlink]

This category selection is shown when a CA/CC carrier is selected in the upper pane category.

Shows Spectrum graphics of carrier aggregation layer of the selected carrier.

Carrier

Shows Spectrum graphics of the selected carrier.

CCDF Graphics

CCDF graphics of the selected carrier in the upper pane is shown in the lower pane.

Drawing options:

Carrier Aggregation [Uplink/PRACH/Downlink]

This category selection is shown when a CA/CC carrier is selected in the upper pane category.

Shows CCDF graphics of carrier aggregation layer of the selected carrier.

Carrier

Shows CCDF graphics of the selected carrier.

Understanding CCDF Curves

Waveform Info and Graphics

Waveform

Welcome to LTE TDD